LPC1347 Not starting program

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1347 Not starting program

1,174件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Chill0309 on Fri Oct 12 14:06:45 MST 2012
I have a prototype LPC1347 which I can program and debug fine using CrossStudio. The application runs when I start debugging, but if I disconnect my SWD cable and power cycle it doesn't run the program from Flash. If I reconnect the SWD cable and start the application manually from CrossStudio without re-programming it starts fine.

Anyone any ideas what I'm missing.

I've got the reset line tied high and have toggled it low to force a restart.
0 件の賞賛
返信
3 返答(返信)

1,148件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Chill0309 on Sat Oct 13 00:41:23 MST 2012
https://rowley.zendesk.com/entries/251134-application-not-starting-up-from-reset-lpc1000
0 件の賞賛
返信

1,148件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Fri Oct 12 14:29:53 MST 2012

Quote: Chill0309
I have a prototype LPC1347 which I can program and debug fine using CrossStudio.



:confused:


Quote:

[B]It doesn't work!  Or, what to do before asking for help[/B]



https://rowley.zendesk.com/entries/50670-it-doesn-t-work-or-what-to-do-before-asking-for-help
0 件の賞賛
返信

1,148件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Chill0309 on Fri Oct 12 14:11:33 MST 2012
I have just realised that simply starting actually performs another download to the device, so I guess it might not be saving to the internal EEPROM?
0 件の賞賛
返信