LPC1343 UART DTR, RST etc how to work

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1343 UART DTR, RST etc how to work

552 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by xsimon on Thu May 12 02:46:30 MST 2011
[SIZE=2]Dear Sir,

I'm facing a problem on LPC1343 UART function, I tested LPC1343 CDC com port sample code from NXP and using flashmagic to verify if possible can output TXD, RXD, DTR, RTS, but only TXD can be output by scope measurement, below is my modification need any one can help me.

void ser_OpenPort (void) {

  NVIC_DisableIRQ(UART_IRQn);

  LPC_IOCON->PIO1_6 &= ~0x07;    /*  UART I/O config */
  LPC_IOCON->PIO1_6 |= 0x01;     /* UART RXD */
  LPC_IOCON->PIO1_7 &= ~0x07;   
  LPC_IOCON->PIO1_7 |= 0x01;     /* UART TXD */
  /* Enable UART clock */
  LPC_SYSCON->SYSAHBCLKCTRL |= (1<<12);
  LPC_SYSCON->UARTCLKDIV = 0x1;     /* divided by 1 */
// Below is copy from void ModemInit( void )
  LPC_IOCON->PIO2_0 &= ~0x07;    /* UART I/O config */
  LPC_IOCON->PIO2_0 |= 0x01;     /* UART DTR */
  LPC_IOCON->PIO0_7 &= ~0x07;    /* UART I/O config */
  LPC_IOCON->PIO0_7 |= 0x01;     /* UART CTS */
  LPC_IOCON->PIO1_5 &= ~0x07;    /* UART I/O config */
  LPC_IOCON->PIO1_5 |= 0x01;     /* UART RTS */

  LPC_IOCON->PIO2_1 &= ~0x07;    /* UART I/O config */
  LPC_IOCON->PIO2_1 |= 0x01;     /* UART DSR */
  LPC_IOCON->PIO2_2 &= ~0x07;    /* UART I/O config */
  LPC_IOCON->PIO2_2 |= 0x01;     /* UART DCD */
  LPC_IOCON->PIO2_3 &= ~0x07;    /* UART I/O config */
  LPC_IOCON->PIO2_3 |= 0x01;     /* UART RI */

  LPC_UART->MCR = 0xC0;          /* Enable Auto RTS and Auto CTS. */   
  return;
}

Thanks!
Ethan
[/SIZE]
0 Kudos
Reply
0 Replies