LPC1313 Peripheral Views Error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1313 Peripheral Views Error

ソリューションへジャンプ
2,813件の閲覧回数
mikesimmonds
Contributor III

I am still using IDE v 7.9 for backward compatibility reasons and the peripheral views only offers the windowed watchdog timer which the 1313 does not have (only the standard watchdog timer).

NB I have selected the correct MCU for the project.

I accept that you will not be releasing any fixes for version 7x, but I would like a confirmation that the error has been corrected in version 8.2 before I evaluate if it is worth exploring an update or not.

Regards, Mike.

ラベル(1)
0 件の賞賛
返信
1 解決策
2,646件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

This appears to be a long standing "issue" with the LPC13xx  SVD file (that forms the basis for populating the register contents of the LPCXpresso IDE's peripheral view) only containing the WWDT peripheral, not a WDT.

Thus there will be no difference in what you see here between LPCXpresso IDE v7.9 and 8.x

I seem to remember that the WWDT is a superset of the WDT though, with just a couple of extra registers. Are you actually seeing errors being triggered when you try to display the WDT/WWDT peripheral?

Regards,

LPCXpresso Support

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
2,646件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

Long standing in that the underlying file has been in use for around 3 years, but noone has ever spotted this issue before.

Regards,

LPCXpresso Support

0 件の賞賛
返信
2,647件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

This appears to be a long standing "issue" with the LPC13xx  SVD file (that forms the basis for populating the register contents of the LPCXpresso IDE's peripheral view) only containing the WWDT peripheral, not a WDT.

Thus there will be no difference in what you see here between LPCXpresso IDE v7.9 and 8.x

I seem to remember that the WWDT is a superset of the WDT though, with just a couple of extra registers. Are you actually seeing errors being triggered when you try to display the WDT/WWDT peripheral?

Regards,

LPCXpresso Support

0 件の賞賛
返信
2,646件の閲覧回数
mikesimmonds
Contributor III

See above.

0 件の賞賛
返信
2,646件の閲覧回数
converse
Senior Contributor V

According to this document:

http://www.nxp.com/documents/data_sheet/LPC1311_13_42_43.pdf 

LPC1313 (and LPC1311) does have the Windowed Watchdog timer...

0 件の賞賛
返信
2,646件の閲覧回数
mikesimmonds
Contributor III

@ Con Verse (ha ha)

Referring to the user manual UM10375:

18.1 How to read this chapter
This chapter describes the WDT block without the windowed watchdog features and
applies to the LPC1300 parts LPC1311/13/42/43.

19.1 How to read this chapter
This chapter describes the Windowed WDT available on the LPC1300L parts LPC1311/01
and LPC1313/01.

@ LPCX Support

I no longer need to debug the watchdog operation, but such sloppy QA scares me from moving away from 'the devil you know'.

Also 'long standing' and still not corrected does not inspire very much confidence.

Regards, Mike.

0 件の賞賛
返信