LPC11U37 / 401 Invalid Part ID + Log

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC11U37 / 401 Invalid Part ID + Log

1,560 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nebarto on Wed Sep 19 23:43:32 MST 2012
I believe this needs to be updated, it seems the /401 and /501 versions are flipped around.
It works if I use /501 settings with my 401 chip. But I am wary of using this long term since the memory mapping is different.

Correct values from UM10462:

LPC11U37FBD48/401 0x0001 7C40
LPC11U37FBD64/501 0x0000 7C40


________________________________________
my error log: (Version: LPCXpresso v4.2.3 [Build 292] [30/05/2012] )


LPCXpresso Debug Driver v4.0 (May 21 2012 21:42:54)
Looked for chip XML file in C:/nxp/LPCXpresso/lpcxpresso/bin/LPC11U37/401.xml
Looked for vendor directory XML file in C:/nxp/LPCXpresso/lpcxpresso/bin/nxp_directory.xml
Found generic directory XML file in C:/nxp/LPCXpresso/lpcxpresso/bin/crt_directory.xml
Emu(0): Conn&Reset. DpID:  BB11477. Info: T1S6RGRIA
SWD Frequency: 3000 KHz. RTCK: False. Vector catch: False.
Packet delay: 0  Poll delay: 0.
Invalid LPC11U37/401 Part ID: 0x00017C40
Known LPC11U37/401 ID(s): 0x00007C40
03: Failed on chip setup: Ec(01). Invalid, mismatched, or unknown part
0 Kudos
Reply
2 Replies

1,536 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by daniel.widyanto on Thu Sep 27 23:59:41 MST 2012
Hi,

As what CodeRedSupport said, LPC11U37FBD48/401 part ID issue has been resolved in LPCXpresso 4.3.0.

Please update your LPCXpresso to the latest version (you are using LPCXpresso 4.2.3)
0 Kudos
Reply

1,536 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Thu Sep 20 05:46:44 MST 2012
This should be fixed in LPCXpresso 4.3.0 ....

http://knowledgebase.nxp.com/showthread.php?t=3652

Regards,
CodeRedSupport
0 Kudos
Reply