LPC11CXX Non Volatile Flash like EEPROM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC11CXX Non Volatile Flash like EEPROM

1,765 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by gopikrishnan47 on Tue Apr 17 07:02:18 MST 2012
Hi,
          I downloaded the AN11008 application note to use the flash like EEPROM for storing user data. The source code available is for Keil IDE. I am using LPCxpresso. porting that code into LPCxpresso creates a lots of trouble. does the code  available for LPCXpresso.
      Else what are the things i have to change in order to make the original code work in LPCXpresso.

Regards,
Gopi Krishnan A.
0 Kudos
Reply
5 Replies

1,637 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ano on Wed Sep 03 05:01:54 MST 2014
I have the same question, but since the from has changed, the link is dead.
Does someone have a working Storage System (EEPROM-like) on the LPC11C24?
Most preferably the NVOL one, described in AN11008.
There is no example in the LPCOPEN2.0  :((

Would be really really gratefull!
0 Kudos
Reply

1,637 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by micrio on Wed Apr 18 18:50:26 MST 2012
I picked that piece out of my larger project.   I can't post the project.
What is the problem with the code?

Pete.
0 Kudos
Reply

1,637 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by gopikrishnan47 on Tue Apr 17 23:13:00 MST 2012
Could you please provide the full project for LPCXpresso-> LPC11C24. the piece of code you have provided is having some trouble.
0 Kudos
Reply

1,637 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by gopikrishnan47 on Tue Apr 17 21:22:43 MST 2012
thanks micrio....
0 Kudos
Reply

1,637 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by micrio on Tue Apr 17 18:41:22 MST 2012
I posted some code that uses the flash to store persistent data.
Here is the thread;
http://knowledgebase.nxp.com/showthread.php?t=2073
0 Kudos
Reply