LPC11C24 LPCXPRESSO BOARD Error during final launch sequence

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC11C24 LPCXPRESSO BOARD Error during final launch sequence

2,397 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by yash_tambi on Wed Apr 13 23:22:39 MST 2016
Hi,

I am using LPC11C24 LPCXPRESSO BOARD for a code development. It was working fine until yesterday when I encountered this error

Error in final launch sequence
Failed to execute MI command:
-target-select extended-remote | crt_emu_cm_redlink -msg-port=50443 -g -mi -2 -pLPC11C24/301 -vendor=NXP -reset= -ProbeHandle=1 -CoreIndex=0 -flash-driver=LPC11_12_13_32K_8K.cfx
Error message from debugger back end:
Remote communication error.  Target disconnected.: No error.
Remote communication error.  Target disconnected.: No error.


The LPC Link (Probe v1.3) does seem to connect to the computer because it shows up in the Connect to Emulator window when I press the debug button on the IDE.

I have tried using a different computer, using a different OS, but got the same problem every time.

Any help would be highly appreciated,

Thanks in advance,
Yash
0 Kudos
Reply
3 Replies

2,297 Views
lpcware
NXP Employee
NXP Employee
bump
0 Kudos
Reply

2,297 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by yash_tambi on Thu Apr 14 04:02:46 MST 2016
This solved the problem, Thanks :)
0 Kudos
Reply

2,297 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by vtw.433e on Thu Apr 14 00:35:29 MST 2016
Try this FAQ:
https://www.lpcware.com/content/faq/lpcxpresso/regaining-debug-access
0 Kudos
Reply