LPC1114/333. Problems Programming Flash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1114/333. Problems Programming Flash

1,065 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by [email protected] on Tue Feb 05 03:19:50 MST 2013
I'm trying to program the flash of my board designed with the LPC1114/333 but I get the next error:

[SIZE=2]Ni: LPCXpresso Debug Driver v5.0 (Dec 18 2012 17:03:37 build 1101)[/SIZE]
[SIZE=2]Pc: ( 0) Reading remote configuration[/SIZE]
[SIZE=2]Nc: Looked for chip XML file in E:/nxp/LPCXpresso_5.0.14_1109/lpcxpresso/bin/LPC1114/333.xml[/SIZE]
[SIZE=2]Nc: Looked for vendor directory XML file in E:/nxp/LPCXpresso_5.0.14_1109/lpcxpresso/bin/nxp_directory.xml[/SIZE]
[SIZE=2]Nc: Found generic directory XML file in E:/nxp/LPCXpresso_5.0.14_1109/lpcxpresso/bin/crt_directory.xml[/SIZE]
[SIZE=2]Pc: ( 5) Remote configuration complete[/SIZE]
[SIZE=2]Ed:02: Failed on connect: Ee(07). Bad ACK returned from status - wire error.[/SIZE]
[SIZE=2]Et: Emu(0): Connected. Was: None. DpID: EDB6. Info: WIN64HS12[/SIZE]
[SIZE=2]Error 0: (null)[/SIZE]
[SIZE=2]Last sticky: 0. AIndex: 0[/SIZE]
[SIZE=2]No MemAp selected[/SIZE]
[SIZE=2]No Speed test[/SIZE]
[SIZE=2]SWD Frequency: 50 KHz. RTCK: False. Vector catch: False.[/SIZE]
[SIZE=2]Packet delay: 0 Poll delay: 0.[/SIZE]
[SIZE=2]Pc: (100) Target Connection Failed[/SIZE]

[SIZE=2][SIZE=3]I'm only able to load the code joining PIO0_1/BOOT [SIZE=2] to ground or k[/SIZE]illing the clock (shortcicuiting XTALIN to ground).[/SIZE][/SIZE]
[SIZE=2][/SIZE]
[SIZE=2][SIZE=3]Has anyone experienced thisproblem?[/SIZE]

[SIZE=3]Thanks[/SIZE][/SIZE]
0 Kudos
Reply
2 Replies

1,043 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Wed Feb 06 07:47:02 MST 2013

Quote: [email protected]

[SIZE=2][SIZE=3]I'm only able to load the code joining PIO0_1/BOOT [SIZE=2] to ground or k[/SIZE]illing the clock (shortcicuiting XTALIN to ground).



Check your debug/reset related connections, as per:

http://support.code-red-tech.com/CodeRedWiki/HardwareDebugConnections

In particular, do you have a pull up resistor on the ISP pin ?

Regards,
CodeRedSupport
0 Kudos
Reply

1,043 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Tue Feb 05 06:56:28 MST 2013

Quote:

[SIZE=2][SIZE=3]Has anyone experienced thisproblem?[/SIZE][/SIZE]

No, I've no 'my board designed with the LPC1114/333' board :eek:

Probably that's a hardware problem (board or SWD) or you've flashed already an invalid program.

Without further informations that's just a guessing game ;)
0 Kudos
Reply