LPC1113 Board Bring Up Issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1113 Board Bring Up Issue

939件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by xfirex on Fri Sep 09 15:22:56 MST 2011
Is there any hardware configurations needed to bring up my LPC1113 board with the chip directly from factory and never been programmed before? I'd pull-up both PIO0_0 (RESET) and PIO0_1 pins but I measured there is no frequency over the XTALIN pin.
0 件の賞賛
返信
3 返答(返信)

931件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Sun Sep 11 14:11:16 MST 2011
As it's name says: Internal :eek:
0 件の賞賛
返信

931件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by xfirex on Sun Sep 11 14:07:45 MST 2011
Where can I measure the IRC clock?
0 件の賞賛
返信

931件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Fri Sep 09 15:36:49 MST 2011

Quote: xfirex
Is there any hardware configurations...



No :)

If it's new it's starting in ISP mode with 12 MHz Internal RC oscillator (IRC) .
0 件の賞賛
返信