LPC1111 invalid part id

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1111 invalid part id

1,128 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by a.stahl on Thu May 31 06:17:11 MST 2012
Hello!

On a new bunch of our boards with the LPC1111FHN33/101, I get:

Invalid LPC1111/101 Part ID: 0x2516D02B
Known LPC1111/101 ID(s): 0x041E502B, 0x2516902B
03: Failed on chip setup: Ec(01). Invalid, mismatched, or unknown part

I checked the chip on the board and it is correctly labeled as LPC1111F/101.

According to the user manual UM10398 Rev.8 page 43, valid part IDs for the LPC1111FHN/101 are 0x041E502B and 0x2516D02B. The /102 only has 0x041E502B.

The IDs 0x0416502B and 0x2516902B are for the LPC1111FHN/201.
So there seems to be a problem with LPCxpresso.

If so, is there a way (config file or something) to change the "known IDs" ?

For now, I changed the project setting to MCU type LPC1111/102. It works, but it "doesn't feel right"... Afaik the /101 and /102 parts differ only in existence of the power profiles.

Andreas
0 Kudos
Reply
3 Replies

1,107 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Thu Jul 19 06:58:57 MST 2012
Thanks for the report.

I actually spotted this when I checked out the original report from a.stahl.  I can confirm that this is fixed for inclusion in releases after 4.2.3.

Regards,
CodeRedSupport
0 Kudos
Reply

1,107 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jvde_oce on Thu Jul 19 03:08:21 MST 2012
[FONT=Arial][SIZE=2]Hello[/SIZE][/FONT]

[FONT=Arial][SIZE=2]I have a similar problem but with a LPC1111FHN33/201 (chip label LPC1111F/201)[/SIZE][/FONT]

[FONT=Arial][SIZE=2]get the next error:[/SIZE][/FONT]
[SIZE=2][FONT=Arial]Invalid LPC1111/201 Part ID: 0x2516902B[/FONT][/SIZE]
[SIZE=2][FONT=Arial]Known LPC1111/201 ID(s): 0x0416502B, 0x2516D02B[/FONT][/SIZE]
[SIZE=2][FONT=Arial]03: Failed on chip setup: Ec(01). Invalid, mismatched, or unknown part[/FONT][/SIZE]

[FONT=Arial][SIZE=2]looking in the UM10398 I see that the Part ID ought to be: 0x0416 502B; 0x2516 902B[/SIZE][/FONT]

[FONT=Arial][SIZE=2]if I select the LPC1111F/202 (witch has the same Part ID: 0x2516902B) the chip will work[/SIZE][/FONT]

[FONT=Arial][SIZE=2]could you fix this one as well [/SIZE][/FONT]

[FONT=Arial][SIZE=2]Thanks,[/SIZE][/FONT]
[FONT=Arial][SIZE=2]Jos[/SIZE][/FONT]
0 Kudos
Reply

1,107 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Thu May 31 08:59:20 MST 2012
Looks like you are correct - the numbers have got transposed at some point. We'll fix this in the next release (ie the release after 4.2.3 which we made earlier today).

Regards,
CodeRedSupport
0 Kudos
Reply