LPC110 Commit Flash Issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC110 Commit Flash Issue

996件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nVideon on Mon Apr 22 15:04:23 MST 2013
I have been using Red Suite 3 for several years and start a new project with an LPC1100. I downloaded the version 5 LPCXpresso and installed it. I can read and write the RAM in the LPC1100 and I can read the flash memory. I wrote a simply program. When I try to debug it, I get a Commit flash error. Any ideas at to what might be wrong? I am using a Red Probe+ as the debug probe.
0 件の賞賛
返信
1 返信

983件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Mon Apr 22 18:10:28 MST 2013

Quote: nVideon
I have been using Red Suite 3 for several years and start a new project with an LPC1100. I downloaded the version 5 LPCXpresso and installed it. I can read and write the RAM in the LPC1100 and I can read the flash memory. I wrote a simply program. When I try to debug it, I get a Commit flash error. Any ideas at to what might be wrong? I am using a Red Probe+ as the debug probe.



Sorry for the inconvenience. With the 5.2.2 release, we converted the rest of the debug utilities to use the loadable flash driver model. Unfortunately, the LPC11_12_13_4K_1K.cfx driver file you require for the LPC1110FD had a build problem. The fix will be included in the next release. In the meantime, you'll find an updated driver file attached to this response. Extract the LPC11_12_13_4K_1K.cfx driver file from the attached archive to the '<install>/lpcxpresso/bin/Flash' folder, overwriting the existing driver file.

Regards,

CodeRedSupport
0 件の賞賛
返信