LPC xpresso error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC xpresso error

5,317件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by IvorNxp on Sun Feb 26 19:41:52 MST 2012
Hi, All
When I click the botton of "Debug", note me a Lpc xpress error. Please find of attachement file of LPC Xpresso error.JPG.
I don't know why note this???
Ivor a nxp member. :)
0 件の賞賛
返信
8 返答(返信)

5,304件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by IvorNxp on Mon Feb 27 21:07:13 MST 2012

Quote: CodeRedSupport
The error is caused by the IDE not being able to find required files. These files are automatically installed along with all other files. So:
- have you deleted any files?
- has your antivirus deleted/quarantined any files?

If this doesn't help, can you post the output from:
Help->Support->Product Information



I am not deleted any files.
My computer not runing antivirus or quarantined any files.

Thank a lot!
By Ivor
0 件の賞賛
返信

5,304件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by IvorNxp on Mon Feb 27 20:59:36 MST 2012

Quote: CodeRedSupport
The error is caused by the IDE not being able to find required files. These files are automatically installed along with all other files. So:
- have you deleted any files?
- has your antivirus deleted/quarantined any files?

If this doesn't help, can you post the output from:
Help->Support->Product Information



information as below:
Plugins and versions:
- com.crt.advproject (4.2.0.201202231813)
- com.crt.config (4.2.0.201202231813)
- com.crt.ctrlcenter (4.2.0.201202231813)
- com.crt.debugcommon (4.2.0.201202231813)
- com.crt.debugmgr (4.2.0.201202231813)
- com.crt.docs (4.2.0.201202231813)
- com.crt.lite (4.2.0.201202231813)
- com.crt.lite.brand (4.2.0.201202231813)
- com.crt.quickstart (4.2.0.201202231813)
- com.crt.redstate (1.0.1.201202231813)
- com.crt.redtracepreview (4.2.0.201202231813)
- com.crt.trueview (4.2.0.201202231813)
- com.crt.utils (4.2.0.201202231813)
- com.crt.vendor.nxp.a7 (4.2.0.201202231813)
- com.crt.vendor.nxp.lpc11 (4.2.0.201202231813)
- com.crt.vendor.nxp.lpc13 (4.2.0.201202231813)
- com.crt.vendor.nxp.lpc17 (4.2.0.201202231813)
- com.crt.vendor.nxp.lpc18 (4.2.0.201202231813)
- com.crt.vendor.nxp.lpc29 (4.2.0.201202231813)
- com.crt.vendor.nxp.lpc31 (4.2.0.201202231813)
- com.crt.vendor.nxp.lpc43 (4.2.0.201202231813)
Product: LPCXpresso
Activation date: N/A
Version: LPCXpresso v4.2.0 [Build 264] [24/02/2012]
Operating system: Windows XP
VM: Java HotSpot(TM) Client VM (32 bit)
About: LPCXpresso:
Version: {0}
Check versions at: http://support.code-red-tech.com/CodeRedWiki/VersionInfo
(c) Copyright Code Red Technologies Ltd. 2006-11. All rights reserved.
Visit http://www.code-red-tech.com
For support on LPCXpresso visit the forum at: http://knowledgebase.nxp.com/lpcxpresso.php
Information on NXP Microcontrollers can be at: http://www.nxp.com/microcontrollers
Information on NXP LPCXpresso can be found at: http://www.nxp.com/lpcxpresso
(c) Copyright Eclipse contributors and others 2000, 2011. All rights reserved.
Visit http://eclipse.org/
This product includes software developed by the
Apache Software Foundation http://www.apache.org/
License type: FULL
Debug limit: 128k
Activation code: B3O5-ATM1-E2A3-LXBU-CYHZ-M0KY-I1PT-E3G5
A FULL copy of LPCXpresso may be used for production.
0 件の賞賛
返信

5,304件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Mon Feb 27 01:08:25 MST 2012
The error is caused by the IDE not being able to find required files. These files are automatically installed along with all other files. So:
- have you deleted any files?
- has your antivirus deleted/quarantined any files?

If this doesn't help, can you post the output from:
Help->Support->Product Information
0 件の賞賛
返信

5,304件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by IvorNxp on Sun Feb 26 20:36:20 MST 2012

Quote: atomicdog
I'm just guessing. In the JPG you posted it looks like there is an extra colon in [FONT=Courier New]file:D:[B][COLOR=red]:[/COLOR][/B]/Program[/FONT]


I am restalled Expresso, but not resolve it. when running
LPCXpresso v4.1.5_219 note a error infomation LPC Xpresso error1.JPG
0 件の賞賛
返信

5,304件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by atomicdog on Sun Feb 26 20:23:25 MST 2012

Quote: IvorNxp
Hi,
  I must to reinstall with "LPC XPRESSO"?

Ivor


I'm just guessing. In the JPG you posted it looks like there is an extra colon in [FONT=Courier New]file:D:[B][COLOR=Red]:[/COLOR][/B]/Program[/FONT]
0 件の賞賛
返信

5,304件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by IvorNxp on Sun Feb 26 20:03:46 MST 2012

Quote: atomicdog
Maybe try reinstalling LPCXpresso? One of the file paths in the JPG looks strange.



did you think this problem is software issues?
0 件の賞賛
返信

5,304件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by IvorNxp on Sun Feb 26 20:02:46 MST 2012
Hi,
  I must to reinstall with "LPC XPRESSO"?

Ivor
0 件の賞賛
返信

5,304件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by atomicdog on Sun Feb 26 19:47:37 MST 2012

Quote: IvorNxp
Hi, All
When I click the botton of "Debug", note me a Lpc xpress error. Please find of attachement file of LPC Xpresso error.JPG.
I don't know why note this???
Ivor a nxp member. :)

Maybe try reinstalling LPCXpresso? One of the file paths in the JPG looks strange.
0 件の賞賛
返信