LPC-link 2 problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC-link 2 problem

3,471件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by zhaichangmin2 on Wed Feb 19 00:43:03 MST 2014
Hi All:
        I use LPC-link 2 as a debugger to debug LPC1768,  the IDE I use is  LPCXpresso v6.1.4_194, 
when I debug a project, the IDE have following problem:

[color=#930][color=#900]       Error in final launch sequence
        Error: Unable to connect wire for probe index 1.
        RedlinkAPI: Wire Ack Fault - target connected?

[color=#930]      Redlink Server will be restarted.
      Please restart your debug session.
      Error: Unable to connect wire for probe index 1.
      RedlinkAPI: Wire Ack Fault - target connected?[/color]
[color=#930]
      Redlink Server will be restarted.
      Please restart your debug session.[/b][/color][/color]
[/color]

I need help, thanks.

0 件の賞賛
返信
6 返答(返信)

3,222件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Tue Jun 17 00:20:50 MST 2014
Few things to try…

Turn the power to the board and the probe off, then try booting your board into ISP mode before starting your debug connection:

http://www.lpcware.com/content/faq/lpcxpresso/regaining-debug-access

Ensure you have shut down any previous debug session. You must close a debug session (press the Red 'terminate' button) before starting another debug session. It is possible that the debug driver is still running in the background. Use the task manager or equivalent to kill any tasks called:
[list]
  [*]redlinkserv
  [*]arm-none-eabi_gdb*
[/list]

Try a different USB cable!

Try a different USB port. If your host has USB3 and USB2, then try a USB2 port. There are know issues generally with motherboard USB3 firmware, ensure your host is using the latest driver from the manufacturer. Note: this is not referencing the host OS driver but the motherboard firmware of the USB port.

If using a USB hub, make sure it is a powered one. And also try a direct connection between the LPC-Link2 and the host computer instead.

Regards,
LPCXpresso Support
0 件の賞賛
返信

3,222件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lukuan on Mon Jun 16 19:54:06 MST 2014
Yes, Because paste of the chip,  LPC-Link2 has no problem.[/quote]

Hello Zhai.
I am having the exact same problem on my EA-OEM-509 (LPC1788-32 developer's kit).
I was able to debug projects for a few days using LPC-Link2 before the same error as yours appears.

Redlink Server will be restarted.
Please restart your debug session.
Error: Unable to connect wire for probe index 1.
RedlinkAPI: Wire Ack Fault - target connected?

May I know what you meant by paste of the chip and how you resolved the problem?
Thanks in advance.
0 件の賞賛
返信

3,222件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by zhaichangmin2 on Sat May 03 21:29:31 MST 2014

Quote: Robermeyer
Did this ever get resolved?


Yes, Because paste of the chip,  LPC-Link2 has no problem.
0 件の賞賛
返信

3,222件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Robermeyer on Thu May 01 15:03:23 MST 2014
Did this ever get resolved?
0 件の賞賛
返信

3,222件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by zhaichangmin2 on Wed Feb 19 01:01:41 MST 2014

Quote: TheFallGuy
This means that LPC-Link2 is unable to find your target over JTAG/SWD.
- is the target connected?
- is JTAG or SWD correctly wired up?
- is the target powered?
- has the target entered a CRP mode?
-
For more information, search the FAQs for Debug Connection.



First,  there is no problem, I can debug project. 
After a period of time this problem appears.
0 件の賞賛
返信

3,222件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Wed Feb 19 00:48:12 MST 2014
This means that LPC-Link2 is unable to find your target over JTAG/SWD.
- is the target connected?
- is JTAG or SWD correctly wired up?
- is the target powered?
- has the target entered a CRP mode?
-
For more information, search the FAQs for Debug Connection.
0 件の賞賛
返信