LPC libraries on different compilers.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC libraries on different compilers.

651 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by PRASAD HEGDE on Sun May 08 23:20:49 MST 2016
Hello,

Problem : I would like to use the LPC library (e.g. USB library) compiled in one 'C' compiler with another 'C' compiler(May be Armcc or IAR compiler) which has the application.
Is this possible? If yes how? will the linker works correctly without any issue?

What is required? : I would like to create a library which will be independent of the 'C' compiler.

Best Regards
Prasad





0 Kudos
Reply
1 Reply

629 Views
lpcware
NXP Employee
NXP Employee
bump
0 Kudos
Reply