LPC libraries on different compilers.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC libraries on different compilers.

673件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by PRASAD HEGDE on Sun May 08 23:20:49 MST 2016
Hello,

Problem : I would like to use the LPC library (e.g. USB library) compiled in one 'C' compiler with another 'C' compiler(May be Armcc or IAR compiler) which has the application.
Is this possible? If yes how? will the linker works correctly without any issue?

What is required? : I would like to create a library which will be independent of the 'C' compiler.

Best Regards
Prasad





0 件の賞賛
返信
1 返信

651件の閲覧回数
lpcware
NXP Employee
NXP Employee
bump
0 件の賞賛
返信