LPC Xpresso Installation problems

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC Xpresso Installation problems

1,351件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Erupter on Mon Apr 23 04:16:29 MST 2012
Hello.
I downloaded LPC Xpresso versions
4.2.0 b264
4.2.2 b275

Both give me an error after installation.
When I launch the program I first get this error window
"Internal error: no vendors found.
Exception"

Then the program appears to work. But if I try to create a new project, I get a "null pointer" exception when selection the MCU.

I tried disabling firewalls and antivirus during install, but didn't solve.
0 件の賞賛
返信
4 返答(返信)

1,341件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Erupter on Mon Apr 23 13:09:08 MST 2012
Using Win7 64, localization english.
System is installed on C:, I tried installing Xpresso on "D:\Program Files (x86)".
0 件の賞賛
返信

1,341件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Mon Apr 23 06:13:31 MST 2012
Can you tell us which version of Windows you are running, and which language? Also, which directory did you install into, and how did you select that directory?

We have a specific check in the installer that should give a warning if you try to install into Program Files. We have tried this on several version of Windows and in various languages, and the check is correct, so we are interested to find out what is different about your installation.
0 件の賞賛
返信

1,341件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Erupter on Mon Apr 23 04:50:52 MST 2012
No I didn't.
Also because I too did not receive any warning during install.

Thank you.
0 件の賞賛
返信

1,341件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Mon Apr 23 04:36:46 MST 2012
Did you read this already ?

http://knowledgebase.nxp.com/showthread.php?t=2288
0 件の賞賛
返信