LPC Xpresso Activation Problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC Xpresso Activation Problem

983件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by kkawula on Thu Jul 14 02:36:43 MST 2011
I'm new user of LPC Xpresso. I've downloaded latest release (4.0.5) and I had generated activation key which is:
C1LU-J2FW-OZFY-P0N4-O4C4-BQA3-B5EQ-LVF3 (it was generated from SN: GQMR-BXJR-NUP0-L1A1-BVH5-DYDS-G2J5-CZPU-KXL5-MRC3)
When I'm trying to active using "help->product activation->Enter  Activation code" it doesn't return any error instead of it LPC Xpresso  show message:  "Licence type: Unregistered (code = -1)"

I had already  run  "cscript.exe" and go thought activation process again but without any results:(.

I was trying to generate lic file by using command crt_emu_cm3_nxp  -info-license but every time it was closed by Windows because of its  internal error.
I enclose lic file and acc file generated by LPC Xpresso while activation process I hope they will be useful.
I'm using a 32-bit Windows Xp operation system.

Has anyone idea how I can fix my problem?
0 件の賞賛
返信
2 返答(返信)

956件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by kkawula on Thu Jul 14 05:51:15 MST 2011
Thank you:) now it's work.
0 件の賞賛
返信

956件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Thu Jul 14 03:35:15 MST 2011
We are receiving an error: "No Script Engine For File Extension VBS"

A google for this error will show lots of hints on how to solve this problem, including:
http://www.winhelponline.com/blog/error-there-is-no-script-engine-for-file-extension-when-running-vb...
0 件の賞賛
返信