LPC-Link2 problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC-Link2 problem

1,370 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Didier123 on Sun Oct 12 05:45:10 MST 2014
Just bought an LPC-Link2 from Mouser.
It gives me the same error when used on 2 different computers that otherwise work fine with LPCXpresso1769 boards or with an Embedded Artists Android Open Accessory mated to a RedProbe.
I tried to reprogram the LPC-Link2 using the configuration tool on this site but it made no difference.
When initially connecting to the debugger, LPCXpresso reports a funky serial number. I have attached screen shots of the window.
I have also attached a screen shot of the error window.

Here are screen shots:
[img]http://www.eds-fl.com/nxp.LPC-Link2_connected.png[/img]
[img]http://www.eds-fl.com/nxp.LPC-Link2_error.png[/img]

Any help appreciated!
0 Kudos
Reply
4 Replies

1,355 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Didier123 on Tue Oct 14 08:28:42 MST 2014
It was indeed the JTAG cable connected backwards. The cable faces towards the inside of the board, rather than the outside like the Red Probe, so that threw me off. The connector actually has pin numbers on the board, I could have checked that...

Thanks!

Didier
0 Kudos
Reply

1,355 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Sun Oct 12 10:34:56 MST 2014
It means exactly waht it says - it cannot find the target. This is normally caused because the JTAG/SWD cable is connected the wrong way round, or your target does not have any power.
0 Kudos
Reply

1,355 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by serge on Sun Oct 12 07:40:14 MST 2014
Have you read the manual and set the correct jumpers?
0 Kudos
Reply

1,355 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Didier123 on Sun Oct 12 05:46:07 MST 2014
Forgot to add I use LPCXpresso 7.4.0
0 Kudos
Reply