LPC-Link2 and LPC-Link ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC-Link2 and LPC-Link ?

973件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by louislo on Fri Mar 14 03:13:58 MST 2014
Is there any significance diffrence for the[ NXP - OM13035 - LPC1115, LPCXPRESSO, EVAL BOARD], if i were to use the linker part only for debugging, compared to the [NXP - OM13054,598 - LPC-LINK2, GENERAL PURPOSE]?.

Previously i have been using the seperated Xpresso board (LPC-Link)  to program and debug LPC2388 but wish to consider for LPC-Link 2 for future debugging.
0 件の賞賛
返信
2 返答(返信)

957件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by louislo on Sun Mar 16 18:10:23 MST 2014
Ouch, too bad. Guess i have to stick with LPC-Link then.
Just saw it from that link. Thanks for the reply!
0 件の賞賛
返信

957件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LabRat on Fri Mar 14 04:44:32 MST 2014
LPC-link2 is faster  :)

But it doesn't support ARM7  :O

http://www.lpcware.com/content/faq/lpcxpresso/lpc-link2-support


Quote:
As of LPCXpresso 7.0.2, LPC-Link2 is a supported debug probe when used with all NXP MCU families EXCEPT

   [color=#f00] LPC2xxx (ARM7)[/color] , LPC3xxx (ARM9)
        [color=#f00]No support for these parts is planned[/color]


0 件の賞賛
返信