LPC-Link2 & CAN

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC-Link2 & CAN

718件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LabRat on Wed Nov 27 06:56:45 MST 2013
We are just thinking about using LPC-Link2 as CAN-Device...

But we couldn't find CAN-pins in LPC-Link2 schematic??

http://www.embeddedartists.com/sites/default/files/support/xpr/link2/LPC-Link-II_Rev_C.pdf

Even Serial Expansion Interface (J3) isn't offering CAN.

Perhaps it's a good idea to add a hint that GPIO5_8/9 (J3-11/12) is CAN0_RD/CAN0_TD  :)
0 件の賞賛
返信
1 返信

704件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by andersrosvall on Fri Nov 29 07:37:08 MST 2013
The schematic has been drawn by NXP long before it was decided to be an LPC4370 as main processor. Hence the generic pin names.
The LPC-Link2 is mainly a debug probe and focus is not on it being an evaluation board. Again, hence the generic pin names.
You are correct that CAN-pins for one channel are available at J3 pin 11/12.
Kind Regards,
Anders @ Embedded Artists
0 件の賞賛
返信