LPC-Link2 & CAN

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC-Link2 & CAN

716 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LabRat on Wed Nov 27 06:56:45 MST 2013
We are just thinking about using LPC-Link2 as CAN-Device...

But we couldn't find CAN-pins in LPC-Link2 schematic??

http://www.embeddedartists.com/sites/default/files/support/xpr/link2/LPC-Link-II_Rev_C.pdf

Even Serial Expansion Interface (J3) isn't offering CAN.

Perhaps it's a good idea to add a hint that GPIO5_8/9 (J3-11/12) is CAN0_RD/CAN0_TD  :)
0 项奖励
回复
1 回复

702 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by andersrosvall on Fri Nov 29 07:37:08 MST 2013
The schematic has been drawn by NXP long before it was decided to be an LPC4370 as main processor. Hence the generic pin names.
The LPC-Link2 is mainly a debug probe and focus is not on it being an evaluation board. Again, hence the generic pin names.
You are correct that CAN-pins for one channel are available at J3 pin 11/12.
Kind Regards,
Anders @ Embedded Artists
0 项奖励
回复