LPC-Link

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC-Link

3,008 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Mike Beach on Mon Dec 07 03:20:27 MST 2009
Hi,

Is the LPC-Link mentioned on the LPCXpresso and Embedded Artists websites really available as a separate item?  It is only ever mentioned as part of a larger LPC1100 or LPC1300 eval board.

Thanks

Mike Beach

Original Attachment has been moved to: 1100010_problem.txt.zip

0 Kudos
Reply
8 Replies

2,726 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rocketdawg on Mon Oct 21 15:59:09 MST 2013

Quote: NXP_USA

My personal experience has been that fiberglass PCBs can be difficult to break even if scored.



Yea, I use an http://www.xacto.com/products/cutting-solutions/blades/classic-blades/Medium-Saw-Blade.aspx
A Dremel cut off wheel works, but puts to much fiberglass in the air.

Fiberglass is not something you want to breathe.  Take it outside, saw, use dust off or wash, wear a mask & gloves, and wash up afterward.
Seriously, inhalation of fiberglass dust can cause problems years later in life.

0 Kudos
Reply

2,726 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by hamza on Mon Oct 21 14:41:06 MST 2013
  .
0 Kudos
Reply

2,726 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_USA on Wed Dec 09 18:20:14 MST 2009

Quote: LPCVictoria
Are there instructions on how to do this?  It is not clear to me how deep the visible line is between the two halves.  Can we just snap the two halves apart?  Or should we score the dividing line with an exacto-knife first? 

David


We recommend using an exacto knife to scrape through the small copper traces between the two sets of holes. Then a 2x8 0.1" pin header could be soldered on the board so allow re/disconnection with jumpers.

My personal experience has been that fiberglass PCBs can be difficult to break even if scored.
0 Kudos
Reply

2,726 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by kendwyer on Wed Dec 09 10:54:06 MST 2009
The LPC-Link is part of the LPCXpresso board but it can be detached and used standalone. See the QSG. Take a look at the picture of the board here: http://www.standardics.nxp.com/lpcxpresso/

Ken
0 Kudos
Reply

2,726 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by amit on Mon Dec 07 22:21:25 MST 2009

Quote: rkiryanov
Is LPCXPresso compatible with J-Link?



Hi,

No, but you can use the LPCXpresso IDE with Red Probe (JTAG probe from Code Red).

Amit
0 Kudos
Reply

2,726 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LPCVictoria on Mon Dec 07 17:57:25 MST 2009

Quote: NXP_USA
Hello Mike,

LPC-LINK is half of the LPCXpresso board. There is a 10-pin debug connector on the LPCXpresso board that can be used to connect to another external target board. To use it, the connections between the two halves of the board(LPC-LINK and LPC1343) need to be cut.



Are there instructions on how to do this?  It is not clear to me how deep the visible line is between the two halves.  Can we just snap the two halves apart?  Or should we score the dividing line with an exacto-knife first? 

David
0 Kudos
Reply

2,726 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rkiryanov on Mon Dec 07 11:41:40 MST 2009

Quote: NXP_USA



Is LPCXPresso compatible with J-Link?
0 Kudos
Reply

2,726 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_USA on Mon Dec 07 11:14:19 MST 2009
Hello Mike,

LPC-LINK is half of the LPCXpresso board. There is a 10-pin debug connector on the LPCXpresso board that can be used to connect to another external target board. To use it, the connections between the two halves of the board(LPC-LINK and LPC1343) need to be cut.
0 Kudos
Reply