LPC-Link with LPC2368

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC-Link with LPC2368

918 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by martint88 on Wed Feb 23 07:53:52 MST 2011
Hello,
We are working on a project with LPC2368 CPU.
Is it possible to program and debug it using the JTAG from an LPCXpresso board? Is there any software tool we have to purchase to do that?
Thank You!
Martin
0 Kudos
Reply
2 Replies

863 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Wed Feb 23 09:10:10 MST 2011
LPC2368 is not supported by LPCXpresso IDE.

However, it *is* support in all variants of Red Suite (full and NXP Edition) , and LPC-Link is a fully supported debug probe and can be used to debug the LPC2368.

Hope that helps,
0 Kudos
Reply

863 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Wed Feb 23 09:02:11 MST 2011

Quote: martint88
We are working on a project with LPC2368 CPU.
Is it possible to program and debug it using the JTAG from an LPCXpresso board?



No. :mad:


Quote: martint88
Is there any software tool we have to purchase to do that?



See:

http://www.code-red-tech.com/products.php#comparison

Perhaps it's possible to use LPC1768 for your project :)
0 Kudos
Reply