LPC-Link not recognised by Win7

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC-Link not recognised by Win7

1,867 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lgosiewski on Fri Oct 05 15:33:14 MST 2012
After pluging in my LPC-Link Win7(64bit) shows it as COOCOX COLINKEX, then tries to find drivers online and fails. During installation of LPCXpresso, Windows asks several times if I'm sure I want to install drivers before it does so, but device still doesn't work after that. I tried to manually show path to driver files (both LPC-Link and COOCOX), but windows didn't recognise them and refused to install.  In device manager it is shown as COOCOX COLINKEX and in device status is written "The drivers for this device are not installed. (Code 28)". What can I do to make it work at last?
0 Kudos
Reply
5 Replies

1,765 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lgosiewski on Sun Oct 07 09:39:02 MST 2012
Sorry to bother you, people. I figured it out. It is in fact COOCOX COLINKEX. I mistook my board with that one - http://www.lpctools.com/lpc11u14.lpcxpresso.aspx
They look similar, but JTAG is slightly diffrent, what I realised by looking at picture of LPCXpresso board.
0 Kudos
Reply

1,765 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lgosiewski on Sun Oct 07 09:19:20 MST 2012
I have LPC DEV KIT-11U14. Never tried to use any JTAG on my computer before, so it shouldn't find old drivers/register entries. When I try to start debugging session in LPCXpresso on some example project, it states, that it didn't find any emulator.  Even installed Ubuntu 12.04 32bit and there is the same problem.
When I try to boot it manually on Ubuntu I get:

dfu-util -l
[I]Found Runtime: [0a5c:2151] devnum=0, cfg=1, intf=3, alt=0, name="UNDEFINED"[/I]

dfu-util -d 0x471:0xdf55 -c 0 -t 2048 -R -D LPCXpressoWIN.enc
[I]Filter on vendor = 0x0471 product = 0xdf55
No DFU capable USB device found[/I]


lsusb
[I]Bus 002 Device 002: ID 1c7a:0801 LighTuning Technology Inc. Fingerprint Reader
Bus 002 Device 003: ID 04f2:b109 Chicony Electronics Co., Ltd
Bus 003 Device 002: ID 0a5c:2151 Broadcom Corp. Bluetooth
Bus 005 Device 005: ID 09da:000a A4 Tech Co., Ltd Optical Mouse Opto 510D
Bus 008 Device 003: ID 05ac:2356 Apple, Inc.
[/I]
When the jumper JP1 is on, instead of
[I]Bus 008 Device 003: ID 05ac:2356 Apple, Inc.[/I]
I get
[I]Bus 008 Device 004: ID 04cc:0003 ST-Ericsson[/I]
and JTAG is switched to mass storage memory with firmware file on it. In that state Win7 recognizes it as "NXP LPC134X IFLASH USB Device" and lists it under "disc drives".

When I plug it on Win7 only red "power" LED is on, while on Ubuntu besides "power" diode, green "D2" LED shines.
I started thinking, that board is malfunctioning, not operating systems. I tried to plug it on another computer with Win7, but it also recognized it as "COOCOX COLINKEX".
0 Kudos
Reply

1,765 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by whitecoe on Sun Oct 07 02:22:56 MST 2012
Never seen a COLINKEX, but it looks like it is an FTDI based probe - whereas LPC-Link uses DFU to install its debug firmware. Thus I don't see how the two could get confused - unless of course you have used COLINKEX on your PC and it has hijacked the LPC-Link VID/PID.

What LPCXpresso board have you actually got (i.e. your LPC-Link)?

What actually happens when you try to start a debug session within the LPCXpresso IDE?

Have you tried booting the LPCXpresso board / LPC-Link manually?

http://support.code-red-tech.com/CodeRedWiki/LPCLinkDiagnostics

HTH!
0 Kudos
Reply

1,765 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by js-nxp on Sat Oct 06 19:42:58 MST 2012
I have just installed it on my new laptop running Win7 64 bits Home Premium without problems.

All of my stuff is run as administrator if that makes any difference.
0 Kudos
Reply

1,765 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by serge on Sat Oct 06 15:33:07 MST 2012
Have you searched this forum (using the sticky thread)?
You should find a lot of usefull information
0 Kudos
Reply