LPC Link interface speed change

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC Link interface speed change

741 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by baton on Fri Oct 07 05:38:08 MST 2011
Hello

I want to lower the data rate of the SWD interface used for debugging (default is 1.2 Mbit/s). I tried to change the value of "maximum wire speed" in debug configuration menu but it did not affect the speed.
Is there something else i have to do?
0 Kudos
Reply
1 Reply

725 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Fri Oct 07 06:10:24 MST 2011
No and Yes:

http://knowledgebase.nxp.com/showthread.php?t=839
0 Kudos
Reply