LPC Link_2 connection issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC Link_2 connection issue

752件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lintovincent88 on Thu Jun 18 22:10:23 MST 2015
Hi NXp,
  we have some connection problem with LPC link2 programmer. we have done lots of projects using nxp lpc13xx MCU using IDE  LPC xpresso v3.6.3_317 since 2012. Now we moved the project to  new platform LPC xpresso v7.2.0_153 & when we tried to program, its showing "02: Failed to connect: Ep(01)  "

the error details:

Ni: LPCXpresso RedlinkMulti Driver v7.2 (May 13 2014 18:12:36 - crt_emu_cm_redlink.exe build 103)
Pc: (  0) Reading remote configuration
Pc: (  5) Remote configuration complete
Ed:02: Failed on connect: Ep(01). Target marked as not debuggable.
Et: Emu(0): Conn&Reset. Was: None. DpID: 00000000. CpuID: 00000000. Info: (null)
Error 0: (null)
Last sticky: 0. AIndex: 0
No MemAp selected
Pc: (100) Target Connection Failed


is there any  setting needed to change while moving from LPC Xpresso v3.6.3 to LPC xpresso V7.2.0 ??
we are using LPC Link 2 programmer.
0 件の賞賛
返信
1 返信

717件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Fri Jun 19 00:40:25 MST 2015
First question, why did you upgrade to a product that is a year old? There have been lots of improvements and fixes to LPCXpresso since v7.2, not least of which is an order of magnitude improvement in flash download speed.

Anyway, please read this FAQ for information on your reported error, and how to resolve it:
http://www.lpcware.com/content/faq/lpcxpresso/target-marked-not-debuggable
0 件の賞賛
返信