LPC-Link - 15: Target error from Commit Flash write

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC-Link - 15: Target error from Commit Flash write

657 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by yoko on Tue Mar 01 19:51:07 MST 2011
Hi,

    I got this error every time I try to debug the LPC1769 Xpresso board.  I cannot debug the board any more.  How can I recover from this ?

15: Target error from Commit Flash write: Et: Flash driver not ready.

My OS is Windows XP.
0 项奖励
回复
1 回复

623 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Tue Mar 01 20:44:45 MST 2011
Please review this thread. You'll find a link to a Code Red FAQ which should help. It sounds like the part is in a bad state (bad PLL setting, disabled debug, etc.) and you'll need to boot the part into the ISP - a known stable configuration.

http://knowledgebase.nxp.com/showthread.php?t=1589

Regards,

CodeRedSupport
0 项奖励
回复