LPC 1769 Design and Controlling.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC 1769 Design and Controlling.

2,021件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Hareesha on Wed Nov 16 04:02:26 MST 2011
Dear Friends,

I am using LPC 1769 ARM Controller in my project (In PCB Design) . I am using LAN8720 Transceiver for Ethernet communication. So please anyone suggest me which Ethernet connector is suitable for my application.???

Still now we are using 8051F120 controller and CP2200 Transceiver with TYCO_6605752-1 Ethernet connector. Shall I use same connector or any other connector which is suitable for LPC1769 Controller???

And on what basis we can choose Ethernet Connector????


Thanks and Regards

Hareesha.
0 件の賞賛
返信
7 返答(返信)

1,962件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Hareesha on Wed Nov 23 06:24:30 MST 2011
Dear Friends,
I am new to this Graphical LCD. In my application I need to display something. So I am preferring Graphical LCD. I went through [B]NHD[/B] Graphical LCD products. How we can calculate as how many character, Number and images can display by that Graphical LCD???.



Thanks & Regards
[I]Hareesha.[/I]
0 件の賞賛
返信

1,962件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by serge on Mon Nov 21 00:55:19 MST 2011
Looks like a good choice, the connector i mean.
When using an lpcxpresso 1769 board then the leds are on board. Of course if you designed your own custom board it is a good idea to incorporate the leds into the connector to see if there is a valid connection and if there is activity. It is a nice to have feature even if it is only to debug faulty connections.
On the other hand those leds are not necessary.
0 件の賞賛
返信

1,962件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Hareesha on Fri Nov 18 05:28:44 MST 2011
[B][FONT=Times New Roman, serif][SIZE=1]Thanks for your suggestions .[/SIZE][/FONT][/B]

[FONT=Times New Roman, serif][SIZE=1][B]Now I am planing to use PULSE JACK Ethernet connector (Series - J0011D01BNL ).It is having LEDs also. In its data sheet application diagram there is no LED connection form CONNECTOR LED pins to LAN8720 Driver LED pins. Is it necessary to give this connection or no need???[/B][/SIZE][/FONT]

[B][FONT=Times New Roman, serif][SIZE=1]for reference:[/SIZE][/FONT][/B]

[FONT=Times New Roman, serif][SIZE=1][B]PULSE JACK Data sheet path:[/B][/SIZE][/FONT]

[FONT=Times New Roman, serif][SIZE=1][B]http://ww2.pulseeng.com/products/datasheets/J403.pdf[/B][/SI...

[FONT=Times New Roman, serif][SIZE=1][B]LAN8720 Driver Data sheet path:[/B][/SIZE][/FONT]

[FONT=Times New Roman, serif][SIZE=1][B]http://www.smsc.com/media/Downloads_Public/Data_Sheets/8720a...

[B][FONT=Times New Roman, serif][SIZE=1]Why i am asking this means In 8051F120 Controller with cp2200 Ethernet controller, we are giving LED connections from Ethernet connector to CP2200. so I am asking. [/SIZE][/FONT][/B]
0 件の賞賛
返信

1,962件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by serge on Thu Nov 17 09:17:02 MST 2011
I used this MagJack (without leds, exists also with leds) for a 10/100 connection.
http://www.belfuse.com/ProdPage-Magjack.asp?pPart=0811-1X1T-06

or just look for Stewart Connector, they have a nice range distributed by f.e. Farnell.
The only things to consider, in my humble opinion and Zero will surely correct me on this if i am wrong, is the speed 10/100 or 1GB and if you want leds in the connector.
0 件の賞賛
返信

1,962件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Wed Nov 16 06:57:30 MST 2011

Quote:

And I need technical details(Data Sheet, Application Diagram.) of that connector.

Are there no distributors or MagJack companies in India?

This MagJack is made in TAIWAN :eek:, as described in its datasheet in link above:

http://www.morethanall.com/products/index/btype_id/9/type_id/106
0 件の賞賛
返信

1,962件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Hareesha on Wed Nov 16 05:57:51 MST 2011
Thanks for your replay.

                 I gone through the link what u have given. From that i understood full overview of Ethernet comm through LPC1769.While reading all links, some links didn't open in my PC. And I didn't get exactly which connector is suitable for PCB to Ethernet cable. And I need technical details(Data Sheet, Application Diagram.) of that connector.


Thanks & Regards

Hareesha.
0 件の賞賛
返信

1,962件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Wed Nov 16 04:07:38 MST 2011
Did you read this?

http://knowledgebase.nxp.com/showthread.php?t=1499
0 件の賞賛
返信