LPC 1313 internal clock

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC 1313 internal clock

809 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tinto on Thu May 03 05:28:19 MST 2012
Hi...

How can I configure LPC1313 to work on internal oscillator? Any example codes? Or could someone help me to configure the registers of LPC1313 to run on internal clock.
0 项奖励
回复
1 回复

779 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_Europe on Fri May 04 06:46:08 MST 2012
Hi Tinto,

Internal RC oscillator is the default clock source at startup, so no external clock source required to boot the MCU. You can read the description of System Clock for LPC1313 in its user manual "Clocking and power control". You may download any application note for LPC1313 to see how it is configured.
http://www.nxp.com/technical-support-portal/50809/56890/application-notes

Also visit our web site www.lpcware.com for other useful information related to LPC1313
0 项奖励
回复