LCPExpresso LCP1768

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LCPExpresso LCP1768

2,305件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by cleber on Fri Jul 08 05:29:33 MST 2011
I am try to write in LPC1114 that i bought whit the KIT LPC-Link LPC1114 but error NullPointerException appear all the time, what i do? I am using the USB behind and and [SIZE=1]
[LEFT]LPCXpresso: [/LEFT]
Version: LPCXpresso v4.0.5 [Build 123] [27/06/2011]
[/SIZE]but nothing.
Please help me.
0 件の賞賛
返信
8 返答(返信)

2,291件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Fri Aug 05 03:12:25 MST 2011
This looks like a corrupted installation. Some of the required files are missing. This has also lead to corrupted projects.

I suggest you
- uninstall your current version, ensuring the directory is completely deleted
- (re)install the latest (v4.0.6)
-  start LPCXpresso with a NEW workspace (empty directory)
- import the examples appropriate for your board and debug
You should have a working system.

If you need your old projects, you can use the Import existing projects options, but after they have been imported, reselect the Target MCU (this will clear the internal cache for the project and re-read the information from the new install). See http://support.code-red-tech.com/CodeRedWiki/ChangingProjectTarget
0 件の賞賛
返信

2,291件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by yanvasilij on Fri Aug 05 01:59:23 MST 2011
here it is
0 件の賞賛
返信

2,291件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Fri Aug 05 01:52:13 MST 2011
please find the file
<workspace>/.metadata/.log
zip it up and post it as an attachment to this thread

(where <workspace> is the directory containing your project)
0 件の賞賛
返信

2,291件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by yanvasilij on Fri Aug 05 01:48:43 MST 2011
This error heppens all time (starting Code red, creating the project etc.). I can't create project  by Code Red
0 件の賞賛
返信

2,291件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by yanvasilij on Fri Aug 05 01:45:22 MST 2011
here the debag log:

LPCXpresso Debug Driver v4.0 (Jul 22 2011 23:32:09)
Looked for chip XML file in E:/Program Files/LPCXpresso_4.0.6_152/lpcxpresso/bin/LPC1768.xml
Looked for vendor directory XML file in E:/Program Files/LPCXpresso_4.0.6_152/lpcxpresso/bin/nxp_directory.xml
Found generic directory XML file in E:/Program Files/LPCXpresso_4.0.6_152/lpcxpresso/bin/crt_directory.xml
Emu(0): Conn&Reset. DpID: 2BA01477. Info: T1S6RGRIA
SWD Frequency: 3000 KHz. RTCK: False. Vector catch: False.
Packet delay: 0  Poll delay: 0.
NXP: LPC1768  Part ID: 0x26113F37
Connected: was_reset=false. was_stopped=false
v Registered license, download limit of 128K
Writing 7468 bytes to 0000 in Flash (assumed clock: 100.0MHz)
Erased/Wrote page  0-1 with 7468 bytes in 1511msec
Flash write Done
nSRST assert (if available)
Executing in user flash.
Stopped: Breakpoint #1
0 件の賞賛
返信

2,291件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Fri Aug 05 01:33:01 MST 2011
As mentioned before, posting your debug log could help to help you :)
0 件の賞賛
返信

2,291件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by yanvasilij on Fri Aug 05 01:13:45 MST 2011
Someone can answer this question? I have this problem too, but my Code Red version is 4.06
0 件の賞賛
返信

2,291件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Fri Jul 08 05:50:11 MST 2011
Could be helpful if you post your DebugLog:

http://support.code-red-tech.com/CodeRedWiki/DebugLog
0 件の賞賛
返信