Jtag connection

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Jtag connection

1,996件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by unnati on Mon Mar 08 23:26:33 MST 2010
hi,

plz tell me the connections of JTAG pins to be connected to the LPC1114.

i can download the program in the target provided in the LPCkit.

but m not able to download the same program in my own target board...it shows error in connection.so let me know the pin connections of JTAG.

i am stuck
0 件の賞賛
返信
4 返答(返信)

1,964件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_Europe on Wed Mar 10 01:17:03 MST 2010
Hi unnati,
Got it working?

Cheers,
0 件の賞賛
返信

1,964件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by unnati on Wed Mar 10 00:38:24 MST 2010
thanx both of u..:)
0 件の賞賛
返信

1,964件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_Europe on Tue Mar 09 07:16:33 MST 2010
Hi unnati,

Please note that the LPC1300 and LPC1100 doesn't have JTAG but SWD only. This is probably not you problem, but is worth while to mention.

Indeed Fig 34 of the getting started guide shows which connections are needed for SWD. Not all pins are needed for the LPC1114, only the  SWDIO, SWCLK, RESET and GND are recommended to connect.

Kind regards,
0 件の賞賛
返信

1,964件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by wrighflyer on Tue Mar 09 04:03:57 MST 2010

Quote: unnati
hi,

plz tell me the connections of JTAG pins to be connected to the LPC1114.

i can download the program in the target provided in the LPCkit.

but m not able to download the same program in my own target board...it shows error in connection.so let me know the pin connections of JTAG.

i am stuck


The pinout of the JTAG header on the LPC-Link is given in the "Getting started" PDF guide
0 件の賞賛
返信