JVM terminated Exit code = 1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

JVM terminated Exit code = 1

1,803件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Lennart on Sat Mar 05 07:52:37 MST 2011
Hello,

New to forum and LPCXpresso.

Downloaded LPCXpresso some time ago.
Following "Getting started with LPCXpresso user guide" I've installed and started LPCXpresso successfully.

When looking for "Blinky Project" for my board with 1769 MCU on it I did not find a blinky project.
Decided to try another example (don't recall which..).
This failed to build, since it was late night I decided to continue some other day.

Next day, trying to launch LPCXpresso this failed with the error message starting with the thread title.
Whether relevant or not, I removed all content from the temporary folder where the project were located when the build failed.
I've since put it back from Recycle Bin with no effect.

Is there an easy fix for this?
Or if this is quicker, can I uninstall LPCXpresso and install it again (still have the install file on my PC). Am I allowed to register my product again?

My board is LPCXpresso LPC1769 Rev. B.
I'm running Windoze XP.

And btw, is there a "Blinky project" for 1769?

Regards,
Lennart
0 件の賞賛
返信
4 返答(返信)

1,683件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Lennart on Sun Mar 06 05:09:12 MST 2011
Tried reinstalling LPCXpresso a couple of times more.
First time I checked "Launch program" and got no error message.
Closing program and starting from shortcut icon failed.
Reinstalled.
Unchecked "Launch program" and tried to start from shortcut. Failed.
Tried to start program from Start->Programs.
This worked??
Closed program and tested shortcut again.
This works??

So, for now all seems OK.
But I'm really confused about this behavior.
0 件の賞賛
返信

1,683件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Sun Mar 06 04:03:20 MST 2011

Quote:

[B]JVM terminated Exit code = 1[/B]

is an Eclipse error

See: [COLOR=#5174a3]http://www.myeclipseide.com/PNphpBB2...pic-t-142.html[/COLOR]



:confused:
0 件の賞賛
返信

1,683件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Lennart on Sun Mar 06 03:26:53 MST 2011
Thanks for the quick reply.

Reinstalled, registered again, loaded "Blinky" for 1768, changed MCU to 1769, built the project and played for a while. Great.
Closed LPCXpresso.

Restarting program leaves me with same error message...
Ideas?
This is tiresome.
0 件の賞賛
返信

1,683件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Sat Mar 05 08:46:45 MST 2011
1. Install latest version of LPCXpresso (3.6.2)

2. Import: LPCXpresso1768_systick (don't forget to clean before build / debug)

3. Don't forget to change MCU setting (= blinking LED)

http://support.code-red-tech.com/CodeRedWiki/ChangingProjectTarget


Quote:

Am I allowed to register my product again?



Yes.

[B]JVM terminated Exit code = 1[/B]

is an Eclipse error

See: http://www.myeclipseide.com/PNphpBB2-viewtopic-t-142.html
0 件の賞賛
返信