JTAG Programming

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

JTAG Programming

1,314件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by bhallett on Fri Apr 30 05:49:54 MST 2010
Hello all,

I am having difficulty in trying to program a LPC1342 device via its JTAG interface, can anyone tell me if this is at all possible if so with what JTAG programming device? It seems rather strange that the chip pinout describes a JTAG input but it does not seem to be able to be used. I want to be able to use this interface purely for programming it not for debug purposes.

Thanks

Barry
0 件の賞賛
返信
4 返答(返信)

1,288件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Tue May 04 06:17:41 MST 2010
AFAIK, the LPC13 family have never had a JTAG deug interface and thus it was probably a docs error.

BTW: I would STRONGLY recommend that anybody building a product with any Cortex-M0, Cortex-M3 part should use SWD/SWV rather than JTAG.
0 件の賞賛
返信

1,288件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by bhallett on Tue May 04 01:59:31 MST 2010
Thanks all for pointing me in the right direction, it is somewhat frustrating that JTAG functionality has been removed (or was never there in the first place) as development has centred around using this interface for programming. Fortunately it is not to late for us to change the design of our product.

Is there any reason why it was specified as having a JTAG interface and then subsequently removed?

Regards

Barry
0 件の賞賛
返信

1,288件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by igorsk on Fri Apr 30 14:48:02 MST 2010

Quote: bhallett
It seems rather strange that the chip pinout describes a JTAG input but it does not seem to be able to be used. I want to be able to use this interface purely for programming it not for debug purposes.


In the latest User Manual there is a following note in the revision history:
"Pin functions TRST, TDO, TMS, TDI changed to R (Reserved) throughout the
document."
0 件の賞賛
返信

1,288件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Fri Apr 30 06:57:52 MST 2010
Lpc1300 does not have a jtag debug interface. You can only use swd to access the chip.
0 件の賞賛
返信