JRE Issues, 7.0.0_92

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

JRE Issues, 7.0.0_92

1,326件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Atheros on Mon Mar 03 10:42:35 MST 2014
I've attached a log. The top portion is when I run lpcxpresso as root, the bottom half is the output when I run as my normal user.

Thanks for any help!

Original Attachment has been moved to: lpcxpresso.txt.zip

0 件の賞賛
返信
4 返答(返信)

1,240件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Atheros on Tue Mar 04 16:54:19 MST 2014
Interesting, now I will have to do a vanilla install and try LPCXpresso 6.12. ATM I can't even get the IDE to launch, let alone debug a program. Even though it's an older version it is great to see that somebody else has it working on Debian.

I know what I'm doing this weekend ;-)

Thanks for the help!
0 件の賞賛
返信

1,240件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Tue Mar 04 15:33:58 MST 2014
Somebody has it working...
http://www.lpcware.com/content/forum/connection-refused-when-trying-debug
0 件の賞賛
返信

1,240件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Atheros on Tue Mar 04 14:46:49 MST 2014
Yes I have the 32 bit libraries installed, i basically followed the user guide.

Perhaps this should be changed to Ubuntu instead of Linux

http://www.lpcware.com/lpcxpresso/downloads/linux
0 件の賞賛
返信

1,240件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Mon Mar 03 11:16:25 MST 2014
Debian is not one of the distros that we support. However, have you installed the 32-bit compatibility libraries? LPCXpresso is a 32-bit application.
0 件の賞賛
返信