Invalid Project Path Warnings

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Invalid Project Path Warnings

1,167 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ian Stroud on Mon Mar 21 04:39:16 MST 2011
I have recently upgraded from LPCXPRESSO 3.6 to 3.6.2.
Initially I installed 3.6.2 alongside 3.6 in folder c:\nxp\lpcxpresso_3.6_2.
Once I was happy with 3.6.2 I uninstalled 3.6 to ensure it was never used again.
However I now get Invalid Project Path warnings when I compile the code because the system is still trying to look in the old 3.6 path.

Hunting through various settings I find a list a include file paths that include the old deleted folders. However this list can't be edited and I can't find any obvious config files that specify these settings.
[ATTACH]357[/ATTACH]
0 Kudos
Reply
2 Replies

1,100 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ex-kayoda on Mon Mar 21 05:10:07 MST 2011
This problem seems to be described already:

http://support.code-red-tech.com/CodeRedWiki/InvalidProjPath
0 Kudos
Reply

1,100 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Mon Mar 21 04:50:22 MST 2011
Try:

http://support.code-red-tech.com/CodeRedWiki/InvalidProjPath
0 Kudos
Reply