Interface external SPI flash with LPC1114

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Interface external SPI flash with LPC1114

1,519 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by vineetrvce on Tue Jun 26 00:30:43 MST 2012
Hello Group,
   Has anyone interfaced the SPI Flash memory (say, 8Mbit) with LPC 111x CPU.
If there is any reference code, please advise.

Thanks,
Vineet.
0 Kudos
Reply
2 Replies

1,467 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Polux rsv on Tue Jun 26 02:47:07 MST 2012
Researchinnovation,

He was not looking for user manuals, but for example code to read Flash memory through SPI. :rolleyes:

vineetrvce,
There are various SPI flash families, with different protocols: 25Pxx, AT45xxx,.... What is your device?
You will find lot of code. Even if it is for other micros, they will be good starting points.

Angelo
0 Kudos
Reply

1,466 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by researchinnovation on Tue Jun 26 02:06:21 MST 2012

Quote: vineetrvce
Hello Group,
   Has anyone interfaced the SPI Flash memory (say, 8Mbit) with LPC 111x CPU.
If there is any reference code, please advise.

Thanks,
Vineet.




Hi...!!!

http://www.lpcware.com/content/nxpfile/um10398-lpc111xlpc11cxx-user-manual-0
http://www.radiolocman.com/datasheet/data.html?di=114799&/LPC1113FHN33
http://www.scribd.com/doc/77048166/ARM-MCU-User-manual-lpc11xx-lpc11cxx


Thanks & Regards....:)
0 Kudos
Reply