Imported Example Error [LPC1768]

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Imported Example Error [LPC1768]

2,809件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ulisses on Wed May 25 19:46:09 MST 2011
I've imported all examples from the LPCXpresso1768.zip.
But nothing seens to work.
That is the build error message when I try to build the LPCXpresso1768_systick project.

**** Build of configuration Debug for project LPCXpresso1768_systick ****

make all
Building file: ../src/cr_startup_lpc176x.c
Invoking: MCU C Compiler
arm-none-eabi-gcc -D__USE_CMSIS=CMSISv1p30_LPC17xx -DDEBUG -D__CODE_RED -D__REDLIB__ -I"C:\Users\Ulisses\Documents\lpcxpresso_3.6\workspace\CMSISv1p30_LPC17xx\inc" -O0 -Os -g3 -Wall -c -fmessage-length=0 -fno-builtin -ffunction-sections -fdata-sections -mcpu=cortex-m3 -mthumb -MMD -MP -MF"src/cr_startup_lpc176x.d" -MT"src/cr_startup_lpc176x.d" -o"src/cr_startup_lpc176x.o" "../src/cr_startup_lpc176x.c"
arm-none-eabi-gcc.exe: CreateProcess: No such file or directory
make: *** [src/cr_startup_lpc176x.o] Error 1
0 件の賞賛
返信
8 返答(返信)

2,794件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Sat Jul 30 01:41:17 MST 2011
When you start LPCXpresso, you need to make sure that the other toolchain is not on the PATH. You can do this by:
- not having the other toolchain on the 'global' PATH, or
- have a batch file that removes the other toolchain from the PATH and then starts LPCXpresso
0 件の賞賛
返信

2,794件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ulisses on Fri Jul 29 07:42:20 MST 2011
You're right about others tools.
I had to uninstall the GNU Fotran and re-install the LPC-Xpresso Code-Red IDE.

But now I have another problem. The EMTDC/Ps-Cad software, that uses the GNU Fortran is not working!!
I can't have both EMTDC/Ps-Cad and LPC-Xpresso in the same PC!!! :confused:
0 件の賞賛
返信

2,794件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Tue May 31 13:42:53 MST 2011
Do you have any other toolkits installed? Also, do you have cygwin installed
0 件の賞賛
返信

2,794件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Tue May 31 12:30:43 MST 2011
Are you using or did you use another GCC version for something else?
0 件の賞賛
返信

2,794件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ulisses on Tue May 31 12:11:48 MST 2011
All default options.

It is working on my Desktop/Win7 64, but it does not work in my Dell Inspiron, with the same OS.
0 件の賞賛
返信

2,794件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Tue May 31 00:19:36 MST 2011
What is the install location you used? Did you try using the default (c:\nxp)?
0 件の賞賛
返信

2,794件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ulisses on Mon May 30 13:50:17 MST 2011
I've tried to re-install everthing lots of time.
Disable Antivirus, Firewall.
Nothing is working.
0 件の賞賛
返信

2,794件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jharwood on Wed May 25 19:55:19 MST 2011
This came up about a week ago.  Take a look at this thread. It seems the problems were resolved eventually.
0 件の賞賛
返信