IDE settings or project settings

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IDE settings or project settings

514件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mne_nado on Mon Feb 15 10:37:51 MST 2016
Hello.
I use LPCXpresso 8.
I create the new project. The project include the function main().

Add new C file. This file read from uart0

I use library lib82x_chip for (read/write) with uart0
Project is compile but does not work.
If I move this code to  the function main(), the project works.
What's wrong ?
0 件の賞賛
返信
0 返答(返信)