IDE V6/V5 Debugger USB peripheral view Issues

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IDE V6/V5 Debugger USB peripheral view Issues

556 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MikeSimmonds on Fri Sep 27 01:29:22 MST 2013
Firstly, the USB view does NOT show the OHCI registers!
This makes debugging my host application rather difficult.
I had to write code to copy these registers to a 'dump' region.

The USB setup registers (on LPC1778) has upto 5 separate clocks to enable.

Unless ALL of these clocks are selected, the USB peripheral view 'collapses'
complaining about an access violation at 2008C204.
Also, a memory view on the register space (2008C000) shows '??'s even when
all clocks are enabled.
NB: Code that reads individual (appropriate) USB registers works perfectly.

This is increadibly sloppy. Depending on the application, we configure for
one of device, host, or OTG.

There should be separate USB view for these cases (to avoid usless clutter)
and they should be viewable when only the relevant clocks are enabled.

Comments please.
Regards, Mike
0 项奖励
回复
0 回复数