IDE 5.14 Debugger Aborts

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IDE 5.14 Debugger Aborts

1,927件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MikeSimmonds on Sat Jan 26 06:56:05 MST 2013
[FONT=Tahoma][SIZE=1]LPCXpresso 5.14 Clean Install [OK]
New empty workspace
Created a new makefile project
Build OK -- no errors

NB: linked to 0x10000000 (i.e. On-Chip SRam)

Debuger starts (refer to [/SIZE][/FONT][FONT=Tahoma][SIZE=1]http://knowledgebase.nxp.com/showthread.php?t=4091).
That link has a screenshot of the debug launch setup.

Press F5 for step, debug session closes.
The console logs seem to imply an internal gbd error occured.

Ziped logs attached.

Mike.

[/SIZE][/FONT]
0 件の賞賛
返信
6 返答(返信)

1,908件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Tue Jan 29 01:52:37 MST 2013
We have reproduced the problem in 5.0.14 and expect it to be fixed in the next release.
0 件の賞賛
返信

1,908件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MikeSimmonds on Mon Jan 28 18:27:39 MST 2013
[FONT=Tahoma][SIZE=2]I noticed in the console logs that a core file was created.
Would it be helpful to send this to you?
If so, where and in which directory tree is it located,
and what is it called?

Mike

[/SIZE][/FONT]
0 件の賞賛
返信

1,908件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MikeSimmonds on Mon Jan 28 09:06:19 MST 2013
[FONT=Tahoma][SIZE=2]The textfile is a complete step by step.
Is a screenshot wanted, if so of what, at what point.

This issue happens for me every time.

Btw, I had been using 4 in the mean time, selecting 'debug' caused the usb drivers to be reinstalled.

Mike
[/SIZE][/FONT]
0 件の賞賛
返信

1,908件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Mon Jan 28 02:18:18 MST 2013
I have built and loaded your application (after fixing your makefile) and been unable to reproduce any problem with GDB. Please describe exactly (step-by-step) how to reproduce the problem.
0 件の賞賛
返信

1,907件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MikeSimmonds on Sat Jan 26 14:43:57 MST 2013
[FONT=Tahoma][SIZE=2]Here is a minimal project. [NB: for the LPC1778]

BTW, new 'Registers' view is a real pain, it always comes up collapsed.
Is there a way to make it behave like 'Core Registers' from 4. I.e alway open
and no hierachy at all.

[/SIZE][/FONT]
0 件の賞賛
返信

1,907件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Sat Jan 26 11:09:11 MST 2013
I can confirm that is a GDB crash (first one I have seen for a long time). Can you post an example that reproduces the problem, so we can investigate.

Thanks
0 件の賞賛
返信