I2c without secondary device

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I2c without secondary device

794件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Kataconov on Fri Sep 09 02:18:25 MST 2011
Hi!
I need to make some current tests. And i need to initialize I2s and constantly send data in 100kHz mode. But I don't have secondary device.
Is there something way to do it?
My device LPC1114-302 (LPCXpresso board).
0 件の賞賛
返信
2 返答(返信)

787件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by OXO on Fri Sep 09 11:15:00 MST 2011
In the title it says I2C, in the post it says I2S......
0 件の賞賛
返信

787件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by atomicdog on Fri Sep 09 09:35:28 MST 2011

Quote:
I need to make some current tests.

Test what?

Quote:
But I don't have secondary device.

You need to buy one in order to do any real testing.

Quote:
Is there something way to do it?

You can use the debugger to manually force the values into registers but I think that would be a waste of your time.
0 件の賞賛
返信