I need help

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I need help

748 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by cinema_effect on Wed Apr 04 02:58:28 MST 2012
Dear colleagues, could you help me with some information?



The help in configuration LPC1769 is necessary. It is necessary to operate ARM c PC through USB. Where it is possible to follow an example of a configuration of a kernel that it worked as USB Device.
Whether there are standard examples?
0 Kudos
Reply
2 Replies

741 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by cinema_effect on Thu Apr 05 00:19:05 MST 2012
In standarts example I didn't found USB DEVICE.

How to operate ARM through computer if I put an operating system on LPC1769, on it I will start USB Device?
0 Kudos
Reply

741 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Rob65 on Wed Apr 04 09:04:32 MST 2012

Quote: cinema_effect

Whether there are standard examples?


The standard examples are in the examples folder.
As explained in the "Getting Started" manual that is opened during installation of the LPCXpresso tools.
0 Kudos
Reply