How to test UART program using LPC xpresso?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to test UART program using LPC xpresso?

1,206件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by sravansreeram on Mon Jun 22 02:38:26 MST 2015
Hi all,
I'm quite new to this, I am using LPC1347 expresso board and lpcopen libraries. I want to test and check the UART program from the LPC open libraries (periph_uart_rb) .
I have little knowledge about gtkterm in ubuntu.
I have set up gtk term with same baud rate as it is in the C code but the message is not being transmitted and received.
Can someone help me out with this?
0 件の賞賛
返信
2 返答(返信)

1,183件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by sravansreeram on Tue Jun 23 22:38:53 MST 2015
Thanks a lot! I tried it and UART is working now.
0 件の賞賛
返信

1,183件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by elektronist on Mon Jun 22 06:09:36 MST 2015
I recommend you to use cutecom.
0 件の賞賛
返信