How to remove invalid include directories

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to remove invalid include directories

1,647件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by curtvm on Thu Dec 16 16:52:54 MST 2010
I have LPCXpresso 3.6, and have been using 3.2, 3.4, 3.5 before. I (just now) noticed in the 'problems' for the builds, I am getting invalid project paths warnings. They refer to paths which refer to the older versions. If I go to the project properties, Paths and Symbols, Includes, I can see the old paths listed but am unable to delete them (delete grayed out). If I uncheck 'show built-in values', they go away, so I assume they are 'built-in' (they all refer to 'include' or 'include-fixed' directories).  How do I get rid of these old paths? (and where are they stored?)

I install each version to c:\lpcxpresso\_3.X
and the workspace remains at c:\lpcxpresso\workspace
(everything works fine)

I also noticed when uninstalling an older version (I uninstalled 3.4), it also deletes the whole start menu folder (which had 3.5, 3.6 shortcuts). I also noticed the other versions are also gone in the add/remove programs. Maybe its already taken care of in the newer versions, but if not maybe the CodeRed people can modify the uninstaller to watch out for newer versions.
0 件の賞賛
返信
3 返答(返信)

1,571件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by larryvc on Sat Feb 19 14:45:06 MST 2011
I have a similar problem in that upon closing a project and then reopening it in the workspace the include path was changed.

from: CMSISv1p30_LPC17xx/inc
to: projectname/CMSISv1p30_LPC17xx/inc

another close and reopen of the project got me this

from: projectname/CMSISv1p30_LPC17xx/inc
to: projectname/projectname/CMSISv1p30_LPC17xx/inc

I have tried to close LPCXpresso rename the projectname.cs file and
restart LPCXpresso and still have the same result.

Any ideas as to how to get back to the original include path CMSISv1p30_LPC17xx/inc .
0 件の賞賛
返信

1,571件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by curtvm on Thu Dec 16 19:19:32 MST 2010
Thanks! I renamed that .sc file, and problem solved.
0 件の賞賛
返信

1,571件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Luis Digital on Thu Dec 16 18:57:03 MST 2010
Hello,

I think you referred to this problem: [B]Warning: Invalid project Path[/B]
0 件の賞賛
返信