How to disable JTAG pins in Debug with SWDIO/SWCLK?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to disable JTAG pins in Debug with SWDIO/SWCLK?

1,704件の閲覧回数
timothymasters
Contributor II

My target is a LPC11U64FBD64/401 which does not allow debug with JTAG, only boundary scan.  So the debug works only through the SWDIO/SWCLK pins. However, the pins associated with JTAG, TCK, TMS etc. are still disabled during debug. 

Is there a way to disable the JTAG and release the GPIO dedicated to JTAG during debug using the SWDIO/SCLK pin?

Thanks

Tim

0 件の賞賛
返信
1 返信

987件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

Please check the below thread and let me know if this helps.

GPIO port difference | www.LPCware.com 


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信