How to activate the Code Read Protection (CRP)?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to activate the Code Read Protection (CRP)?

3,165 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nerd62 on Fri Jun 11 00:50:21 MST 2010
Hi professionals,

Does anybody know an easy way to activate Code Read Protection (CRP) at LPC11xx? We want to protect our IP against piracy. How can I write CRP level 2 into flash location 0x000002FC? When CRP2 is enabled is it then further possible to abuse a flash sector as an "EEPROM"?

Thanks in advance, nerd62  ;-)
0 Kudos
Reply
3 Replies

2,993 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by kendwyer on Fri Jun 11 20:51:44 MST 2010
With any of CRP levels, IAP calls can be still used to program the flash. Be careful with CRP3, a good idea is to insert a 'backdoor' as detailed in the following AN: http://ics.nxp.com/support/documents/microcontrollers/zip/an10851.zip
0 Kudos
Reply

2,637 Views
azzurrodante
Contributor I

sorry were i can find link AN10851.zip ?   link is changed  

best regards 

0 Kudos
Reply

2,993 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by renan on Fri Jun 11 04:07:49 MST 2010
There is an example for LPC13XX series that shows how to enable CRP.

http://ics.nxp.com/support/lpcxpresso/

Renan
0 Kudos
Reply