How does one get a backtrace in LPCXpresso?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How does one get a backtrace in LPCXpresso?

1,250件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Fklein23 on Tue Jul 22 14:07:18 MST 2014
I am running the free version of LPCXpresso v7.2.0, Build 153, 2014-05-19
We are cross-developing under Windows 8.

I am new to this eclipse platform, and cannot figure out how to get a backtrace.
I am a lot more familiar with command-line gdb under Linux. If I could see the command window, I could just type "bt".
But I can't figure out how to display the command line.

I need to be able to determine from where a function call originated. I know there are additional difficulties with backtracing from inside an exception handler, but that question can wait until another day.

Anyone out there know the "secret handshake" for teasing a simple function call backtrace out of this system?

Thanks,
Frank
0 件の賞賛
返信
2 返答(返信)

1,200件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Fklein23 on Wed Jul 23 06:36:31 MST 2014
Oh. I see it now. I am embarrassed that this has been sitting in front of me for days now and I didn't even recognize it for what it was.
Oops, and thanks for helping me see the obvious.
0 件の賞賛
返信

1,200件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Tue Jul 22 14:54:42 MST 2014
The stack backtrack, aka the call stack, is shown in the Debug view. See section 4.4.2 in the User Guide.
0 件の賞賛
返信