Hardware break point

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hardware break point

1,068 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by affonpign on Wed Oct 05 19:54:41 MST 2011
Hello everybody,

How can I set a hardware break point in the LPCXpresso IDE?

Regards,
affonpign
0 Kudos
Reply
2 Replies

1,045 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by affonpign on Wed Oct 12 02:19:57 MST 2011
Can you explain then how it works. You say that if I add a blue dot breakpoint in the IDE a hardware breakpoint is set. I can set a lot of blue dot breakpoints and I do not think that the uC has so many of them.

Thanks for your help

Regards,
affonpign
0 Kudos
Reply

1,045 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Thu Oct 06 00:36:11 MST 2011
If your code is in flash, then LPCXpresso IDE will automatically use a hardware breakpoint.

Regards,
CodeRedSupport.
0 Kudos
Reply