HEAP problem stops build

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HEAP problem stops build

1,794 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by deBoogle on Wed Oct 05 06:07:14 MST 2011
Hi guys,

I have literally just re-installed Xpresso after a 6 month abscence and I am trying to use the LPC1343 example projects to check my setup but I get the following arror on building the Blinky project:

C:\nxp\LPCXpresso_4.0.6_152\lpcxpresso\msys\bin\sh.exe: *** Couldn't reserve space for cygwin's heap (0x71110000 <0x2380000>) in child, Win32 error 0
make: *** [src/cr_startup_lpc13.o] Error 1

Any ideas why I am getting this, especially from an example project which I would expect to just work!

Many thanks
de Boogle
0 Kudos
Reply
6 Replies

1,706 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Mon Apr 07 18:04:38 MST 2014
For future reference, here is the current version of the FAQ:

http://www.lpcware.com/content/faq/lpcxpresso/virtual-alloc-pointer-null-error

Regards,
LPCXpresso Support
0 Kudos
Reply

1,706 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by geeus81 on Mon Apr 07 15:06:08 MST 2014
This post help me out

Thank you all involved :)
0 Kudos
Reply

1,706 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by whitecoe on Wed Oct 05 07:46:19 MST 2011

Quote:

I did have a quick search on the Forum for this issue but couldnt see anything.

You obviously didn't search very hard :p

Entering "Couldn't reserve space for cygwin's heap" into the google search suggested in the sticky "*** Searching the LPCXpresso Forum and Code Red's FAQ site ***" post at the top of the forum gives multiple hits which take you straight to the answer :)
0 Kudos
Reply

1,706 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by deBoogle on Wed Oct 05 06:37:32 MST 2011
Hi,

I did have a quick search on the Forum for this issue but couldnt see anything.

Thanks for the fast response, I would give you a reputation point but it says I have given you too many already. LOL.  You must work to hard if I have given you so many!

Thanks again
deBoogle
0 Kudos
Reply

1,706 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Wed Oct 05 06:24:31 MST 2011
That's a known problem :)

Solution:

http://support.code-red-tech.com/CodeRedWiki/VirtualAllocPointerNull?highlight=%28cygwin%29

And BTW: Latest version is  v4.1.0 :eek:
0 Kudos
Reply

1,706 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Wed Oct 05 06:23:50 MST 2011
Try this:

http://support.code-red-tech.com/CodeRedWiki/VirtualAllocPointerNull?highlight=%28cygwin%29
0 Kudos
Reply