Get rid of LPCXpresso built-in include paths

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Get rid of LPCXpresso built-in include paths

747件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by pkold on Tue May 01 05:11:29 MST 2012
How do I get rid of the built-in include paths?
In Project->Properties->C/C++ General->Paths and Symbols under "Additional Assembly Source Files" and "GNU C" 3 include folders are always present and the "Delete" button is grayed so they can't be deleted from here.
The folders are named something like:
..arm-none-eabi/4.5.1/include
..arm-none-eabi/4.5.1/include-fixed
..arm-none-eabi/include

I prefer to manually control which folders are searched.
0 件の賞賛
返信
1 返信

728件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by pkold on Tue May 01 05:51:42 MST 2012
Never mind - found it myself
So this is what "Properties->C/C++ Build->Discovery Options" are used for
0 件の賞賛
返信