Generic build question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Generic build question

746 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ECamino on Thu Mar 14 11:26:09 MST 2013
Hi,

I can build my project fine in debug. When I try to build in release, I get:

[LEFT]In function `malloc':[/LEFT]
alloc.c.text.malloc+0x78): undefined reference to `_sbrk'

I researched the error on CR site. It seems that to build the release, the setting under tool settings for Target has to be Redlib, Redlib, and Redlib (semihost), under MCU Linker.

But the debug version builds Redlib, Redlib, Redlib (none).
If host/semihost has to do with debugging support, then why does release not build with MCU Linker set to Redlib (none)?

I have not modified linker script.

EC
[SIZE=2][/SIZE]
0 Kudos
Reply
1 Reply

724 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ex-kayoda on Fri Mar 15 02:13:03 MST 2013
Different libraries provide different functions, that's not reduced to debug functions :)

Redlib(nohost) is useful for memory- (malloc) and string (memcopy) functions ;)

Default library settings of your project are generated while Project Wizard is generating your project :)

So if you generate a LPCXpresso Semihosting project, it's using Redlib(semihost).

But that's just default setting. If you want another library, change it :eek:

See : http://www.support.code-red-tech.com/CodeRedWiki/LibraryVariants
0 Kudos
Reply